|
(Read-Write) Set and query the time average mode. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<bool> |
Time average state. Choose from: OFF or 0 - disables the time average. The Average Time state will automatically switch to OFF when the Average Duration is set. See :CHSCanner:SWEep:AVERage:DURation ON or 1 - enables the time average |
|
Examples |
:CHSC:SWE:AVER:TIME[:STAT] ON */Sets the time average to ON :CHSC:SWE:AVER:TIME[:STAT] 0 */Sets the time average to OFF |
|
Query Syntax |
:CHSC:SWE:AVER:TIME[:STAT]? */queries the time average state |
|
Return Type |
boolean |
|
Default |
OFF or 0 |
Last Modified:
|
26mar2024 |
New command (A.13.00) |